FB#.RESKTR

Description

This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.

The value is obtained from the resolver data sheet.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.001 to 50.000

Default Value

0.5

Data Type

Float
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
FB1.RESKTR

3500h

04h

Unsigned16

-

1000:1

Read/Write

No

FB2.RESKTR

3501h

04h

Unsigned16

-

1000:1

Read/Write

No

FB3.RESKTR

3502h

04h

Unsigned16

-

1000:1

Read/Write

No

FB4.RESKTR

3503h

04h

Unsigned16

-

1000:1

Read/Write

No

FB5.RESKTR

3504h

04h

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.RESKTR

30140

75BC

Unsigned16

Read/Write

-

FB2.RESKTR

30141

75BD

Unsigned16

Read/Write

-

FB3.RESKTR

30142

75BE

Unsigned16

Read/Write

-

FB4.RESKTR

30143

75BF

Unsigned16

Read/Write

-

FB5.RESKTR

30144

75C0

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.RESKTR

30140

Float

Read/Write

-

FB2.RESKTR

30141

Float

Read/Write

-

FB3.RESKTR

30142

Float

Read/Write

-

FB4.RESKTR

30143

Float

Read/Write

-

FB5.RESKTR

30144

Float

Read/Write

-